Technical FAQs

Ask a Question

What meter is used in the Powerpact 4 incoming metering extension enclosures MG64M, MG66M or MG88M?

The Powerpact 4 incoming metering extension enclosures MG64M, MG66M & MG88M come complete with a PM5111 meter.

The PM5111 has the following functionality:
  • I, V, F Energy, PF
  • THD and Min/Max readings
  • Pulsed and Modbus outputs for energy monitoring
Was this helpful?
What can we do to improve the information ?