Technical FAQs

Ask a Question

Will the current range of RCD incomers fit the old AMG or BMG distribution boards?

The current range of RCD incomers ( Acti 9) will not fit into the old AMG or BMG distribution boards which were last manufactured around 1989/90.

The reason they do not fit is that the position and dimensions of the terminals are different.
Was this helpful?
What can we do to improve the information ?