Technical FAQs

Ask a Question

What meter is used in the Isobar metering extension enclosure SEA9BNKWH?

The Isobar metering extension enclosure comes complete with a A9MEM3255 meter.

The meter has the following functionality:
  • Electrical parameters of I, V, P
  • Four quadrant energy measurement
  • Pulsed and Modbus outputs for energy monitoring
Was this helpful?
What can we do to improve the information ?