Technical FAQs

Ask a Question

What are the maximum number of fault operations Ringmaster and GenieEvo will clear

The number of faults that a circuit breaker can clear will depend on the level of fault being interrupted.

Ringmaster: -
  • 16kA - the circuit breaker is designed to clear a maximum number of 11 faults at 16kA 
  • 21kA - the circuit breaker is designed to clear a maximum number 10 times at 21kA
     

GenieEvo is designed to clear a maximum of 100 faults at 25kA.

The fault rating of the unit is detailed on the unit rating plate.

 

Was this helpful?
What can we do to improve the information ?