Technical FAQs

Ask a Question

ION7300 series meter - kWh reading resetting to 0 after reaching 10,000,000

Regarding the Energy Rollout settings, the default value for the ION7350 is 10,000,000 but this value can be increased anytime using ION Setup, just open the setup assistant and navigate to Basic Setup > Rollover. The limit for this register is really high so you can set to up to 999,999,999 if needed

 
Was this helpful?
What can we do to improve the information ?