Technical FAQs

Ask a Question

Can PVC cables be used with expanding foam IMT23029, will the foam degrade the material whilst curing?

IMT23029 - Is safe to use with PVC cables and cable clips during the curing process of the foam this will not harm the cabling like some foams can tend to corrode material, attached datasheet states that this can be used with cable and clips.
Was this helpful?
What can we do to improve the information ?