Technical FAQs

Ask a Question

What are the advantages of Modbus TCP/IP vs. Modbus Serial line protocol?

When it comes to choosing a network for your device, Modbus TCP/IP offers several significant advantages:
  • Simplicity: Modbus TCP/IP simply takes the Modbus instruction set and wraps TCP/IP around it.
    If you already have a Modbus driver and you understand Ethernet and TCP/IP sockets, you can have a driver up and running and talking to a PC in a few hours.
    Development costs are exceptionally low. Minimum hardware is required, and development is easy under any operating system.

     
  • Standard Ethernet: There are no exotic chipsets required and you can use standard PC Ethernet cards to talk to your newly implemented device.
    As the cost of Ethernet falls, you benefit from the price reduction of the hardware, and as the performance improves from 10 to 100 Mb and soon to 1 Gb, your technology moves with it, protecting your investment.
    You are no longer tied to one vendor for support, but benefit from the thousands of developers out there who are making Ethernet and the Internet the networking tools of the future.
    This effort has been complemented opportunely with the assignment of the well-known Ethernet port 502 for the Modbus TCP/IP protocol.

     
  • Open: The Modbus protocol was transferred from Schneider Electric to the Modbus Organization in April 2004, signaling a commitment to openness.
     
  • The specification is available free of charge for download, and there are no subsequent licensing fees required for using Modbus or Modbus TCP/IP protocols.
    Additional sample code, implementation examples and diagnostics are available on the Modbus TCP toolkit, a free benefit to Modbus Organization members and available for purchase by nonmembers.
     
  • Availability of many devices: Interoperability among different vendors' devices and compatibility with a large installed base of Modbus-compatible devices makes Modbus an excellent choice.
Was this helpful?
What can we do to improve the information ?