Technical FAQs

Ask a Question

How do the different versions of MTZ breakers connect to Ethernet?

We provide the following ways to connect MTZ to Ethernet:

For withdrawable MTZ (most probably Playbook3), 2 ways are possible:
  • 1) Use ULP port (standard) + EIFE (Embedded IFE, optional), providing an immediate ready-to-use Ethernet connection.
  • 2) Use ULP port (standard) + IFE or IFE gateway (optional)
For fixed MTZ (most probably Playbook1), you can use the ULP port (optional) + IFE or IFE gateway (optional).

See Attachment:
Was this helpful?
What can we do to improve the information ?