Technical FAQs

Ask a Question

Is it possible to add side instantaneous auxiliary contact blocks to the Tesys D DC coil contactors and relays?

On the Tesys D range, the DC coil contactors and the DC coil relays (both standard and low consumption versions) only allow front mountable auxiliaries.
The part numbers LAD8N11, LAD8N20 and LAD8N02 will fit only on the contactors and relays with AC coil.

Was this helpful?
What can we do to improve the information ?