Technical FAQs

Ask a Question

Q: Is the Masterpact MTZ application available on both Google/Android and Apple iOS platform?

A: YES, both Android and iOS platform are available.

As the iOS platform does not allow to use NFC for any external applications (only for Apple Pay application), the iOS version will not support NFC use cases. In this case, Bluetooth will be the only way to support Crisis / Diagnosis functions of MTZ trip unit.

Unlike NFC technology, Bluetooth technology needs power on the Micrologic to work. Therefore, it’s necessary to use pocket battery in addition to iOS platform to be able to use Crisis / Diagnosis functions when there is no power on MTZ. (Pocket battery not necessary with Android platform in NFC communication mode)
 
Was this helpful?
What can we do to improve the information ?