Technical FAQs

Ask a Question

How to interact with MTZ?

To interact with MTZ, different options are offered to fit different usage scenario and customer habit, including serveral innovative new ways to interact.

 
  User Interface Via To Power by
(1 of these)
Physical
contact CB
Working
Distance
Co mission Local HMI Pushbutton In service
24V
VPS
Yes Local
Local HMI Pushbutton Pocket battery Yes Local
PC / Ecoreach USB PC Once
(USB Plug)
3m
(USB Cable)
Operation Smartphone Bluetooth In service
24V
VPS
Pocket battery
Once
(Bluetooth
activation)
10m
Smartphone NFC None None 10m
Smartphone QR Code None None 10mm
Monitoring PC / IFE
webpage
Ethernet In service
24V
None Distant
PC / SCADA Ethernet In service
24V
None Distant
PC / Com'X
webpage
Ethernet or
Zigbee
In Service
24V
None Distant

MTZ Communications posibilities
Was this helpful?
What can we do to improve the information ?