Technical FAQs

Ask a Question

What are the error codes on Powerlogic PM5000 meters?

If you come across an error code on your PM5000 meter please see below 
 
0003 hex : RAM failure    
0005 : NVRAM failure    
0009 : RTC failure      
0011 : Calibration failure    
0031 : Clipping detected    
0041 : Over running energy pulse output  
0081 : Back up Ram/ Vbat Fail    
0101 :Language file incompatibility   
Was this helpful?
What can we do to improve the information ?