Technical FAQs

Ask a Question

Can the displays for the PM700 and PM800 range of panel mounted power meters be purchased separately?

No, the displays for the PM700 and PM800 range of panel mounted power meters are not available separately. 
There are a range of PM800 meter which are the meter unit only with no built on display ( eg PM8##UMG= power meter with no display) and they require a remote display unit ( PM8RDMG = remote display).
Was this helpful?
What can we do to improve the information ?