Technical FAQs

Ask a Question

Do the Acti9 Single phase Split metered boards (SEA9AN14S14 , SEA9AN10S10 & SEA9AN6S6) come with incomer and meters fitted?

Yes the the Acti 9 Single phase split metered boards (SEA9AN14S14, SEA9AN10S10 & SEA9AN6S6) come with incomer and two meters fitted as standard.
SEA9AN14S14 comes with meters A9MEM2110
SEA9AN10S10 comes with meters A9MEM2110
SEA9AN6S6 comes with meters A9MEM2010
Was this helpful?
What can we do to improve the information ?