Technical FAQs

Ask a Question

On the Prisma P range, does the part number 08676 allows mounting 1 or 2 fans?

This roof was redesigned in 2014. In old catalogues you will find the version that was sold back then, and that one allowed 2 fans.
The current one only allows 1 fan to be mounted.
If you need two fans, you can use the IP54 version part number 08678.
 
Was this helpful?
What can we do to improve the information ?