Technical FAQs

Ask a Question

Are bolts supplied with the snap-in nuts part no LV429234 and LV430554?

Yes bolts are supplied with the snap-in nuts ( set of 12)
Was this helpful?
What can we do to improve the information ?