Technical FAQs

Ask a Question

How to define the part number of a power pact 4 panel board?

In this Range there are Top and Bottom entry Panel Boards so firstly you need to take into consideration the type of installation I.E where the incoming mains cable enters the panel board and where the outgoing circuits will be leaving the Panel Board. Once this is decided you can then proceed to the relavent secton of the Acti 9 Catalouge which you can see from the attached PDF Bottom Entry Distribution Boards are in section 8 page's 6 & 7  and Top entery Panel boards are section 8 page's 8 and 9.

The part numbers for the five variants of the Bottom Entry panel boards have a part number consisting of Letters and numbers For example MG8C12.
The part numbers for the four variants of the Top entery panel boards have a part number consisting of Letters and numbers For example MG8C12T

This is where care should be taken not to confuse the the two part numbers as one is Bottom Entry and The other is Top Entry should the part numbers be misinterpreted. you could have a Distribution Board that will not suit the intended installation.


 
Was this helpful?
What can we do to improve the information ?