Technical FAQs

Ask a Question

Can the trip units be set between settings?

The NSX thermal magnetic trips can only be set at the incrament settigs provided, they cannot be set mid way between points. If they are set between two points the mccb will set to the minimum setting out of the two.
Was this helpful?
What can we do to improve the information ?