Technical FAQs

Ask a Question

Can a single pole NSX have a Micrologic trip unit?

Unfortunately Micrologic trips are only available in 3 or 4 pole versions.
Single pole NSX breakers are Thermal Magnetic trips only.
A solution to this would be to use a 3 pole Micrologic 2 and use just the one phase.
If you choose this option, you would need to select the frame size eg. NSX100, NSX160, or NSX250, then which MCCB Rating and what Micrologic you require.
Was this helpful?
What can we do to improve the information ?