Technical FAQs

Ask a Question

Will the NSX range of MCCB's e.g. LV429630 trip under fault when the toggle is locked ON position?

The NSX range of breaker will still trip under fault conditions even if the toggle is locked in the ON position.
Was this helpful?
What can we do to improve the information ?