Technical FAQs

Ask a Question

Can a motor mechanism be fitted to the MGP4003X & MGP6303X?

The Powerpact 4 panel boards cannot have motor mechanisms fitted to the 400A and 630A breakers. This is due to the panelboard door not being able to be closed.
Was this helpful?
What can we do to improve the information ?