Technical FAQs

Ask a Question

What is the highest rated available for the I Line range of panel board?

The I Line range of panel boards go up to 600 / 630 Amps. For higher amperage ratings use the Powerpact 4 range board up to 1600A
Was this helpful?
What can we do to improve the information ?