Technical FAQs

Ask a Question

How to program pulsed output on PM5000 meters, PM5111 PM5341 PM5561?

It is not possible to set the pulse setting through meter front display, alternatively use  ION setup software.
Download from Schneider Electric website, using the link

The firmware on the meter should be 1.4.7 . and the meter must be unlocked.
User guide on programming the output can be found attached to this FAQ
Was this helpful?
What can we do to improve the information ?