Technical FAQs

Ask a Question

Can the displays for the PM700 and PM800 range of panel mounted power meters be purchased separately?

No, the displays for the PM700 and PM800 range of panel mounted power meters are not available separately.  There is a remote display unit for the PM800 which is the PM8RDMG but this is a remote display for the PM800 power meter unit only with no display.
Was this helpful?
What can we do to improve the information ?