Technical FAQs

Ask a Question

Is it possible to join 2 single phase Acti9 distribution boards on top of each other?

It is not possible to join 2 single phase distribution boards on top of each other as we do not offer a joning kit 

Solution

It is possible to join 3 phase boards on top of each other, depending on the number of ways required you could use 2 x Three phase Acti9 Distribtuioin boards, single phase the supply and then use the joining kit to suit

e.g. For 2 x 6 Way boards on top of each other you would use the below

SEA9BN6 x 2 (6 Way Three Phase Distribution Board)
SEA91253N x 2 (125A Switch for both boards)
SEA9125SPEV  x 2 ( Single phasing kit allowing you to feed all busbars in the Distribution Board with a single phase)
SEA9BNTJKN x 1 (This is the Joining Kit required)
 
Was this helpful?
What can we do to improve the information ?