Technical FAQs

Ask a Question

How to define the part number of Isobar distribution board?

To define the reference of an Acti9 Isobar distribution board there are some pointers to take into consideration i.e if the distibution board is going to be single phase or three phase if it is a single phase distribution board (type A) then in our cataloluge section one page 4 to 6 also see FAQ Number FA288620 and if its three phase distribution board (type B) again in section one page 8 to page 15 also see FAQ Number FA288624
Was this helpful?
What can we do to improve the information ?