Technical FAQs

Ask a Question

What is the replacement of V40H RCBO?

The V40H has no direct replacement

The new RCBO's will not fit in place of these

The best solution is to use a Acti9 iC60H MCB combined with a Vigi Module (A9V02663) for 30mA - in total this is 3 modules

NOTE : You will also require a copper link to adapt the board to accept the new MCB - Part number for a pack of 10 links is BCL

Was this helpful?
What can we do to improve the information ?