Technical FAQs

Ask a Question

What are the dimensions of Isobar A type distribution board?

The dimensions of Isobar distribution boards are dependant on the type of distribution board and number of it's outgoing ways.
The table below illustrate the dimensions of the current distribution boards of which references start with SEA9AN


 
Was this helpful?
What can we do to improve the information ?