Technical FAQs

Ask a Question

What is the control voltage of relays ABR7S33 and ABR7S37?

The control voltage of ABR7S33 and ABR7S37 relays is 24 VDC. 

Please see attached data sheet for more details.

Note:  There was a printing error in the Premium 2008 catalogue, page 8/15: This should read 24 V, not 2 V.
Was this helpful?
What can we do to improve the information ?