Technical FAQs

Ask a Question

Can I connect a Magelis display unit directly to a Zelio module?

From version V1.3 onwards, Vijeo Designer Lite software incorporates the communication protocol with Zelio Logic smart relays.

This communication protocol can only be used on compact display units and terminals with a printer link (XBTN401, XBTR411, XBTRT511) and in combination with the new communication cable for Zelio Logic SR2CBL08. This cable is used to connect the terminal's Mini-Din printer port to the programmable module's integrated port. No external Modbus communication module is therefore required to implement this solution. 


Was this helpful?
What can we do to improve the information ?