Technical FAQs

Ask a Question

What are the possibilities for replacing the DC coils of the LC1D type Tesys D contactors?

Contactor rating 9 A to 38 A
A DC coil cannot be replaced, typical contactor part number LC1D09BD to LC1D38BD.
 

Contactor rating 40 A to 65 A
The coil can be replaced on Tesys D contactors sold between 2001 and 2009, typical part number LC1D40BD to LC1D65BD.
 

On the new Everlink Tesys D contactors sold since 2009, typical part number LC1D40ABD to LC1D65ABD, the coil cannot be replaced

Contactor rating 80 A to 150 A
The coil can be replaced on Tesys D contactors sold since 2001.
 

Was this helpful?
What can we do to improve the information ?