Technical FAQs

Ask a Question

Which Magelis terminals are managed by Vijeo Designer Lite?

Vijeo Designer Lite configuration software manages the following Magelis terminals:
  • XBTN200, Terminal equipped with an alphanumeric display unit with 2 lines x 20 characters.
  • XBTN400 XBTNU400 XBTN401 XBTN410, Terminals equipped with a matrix display with 4 lines x 20 characters.
  • XBTR400 XBTR410 XBTR411, Terminals equipped with a matrix display with 4 lines x 20 characters and keypad.
  • XBTRT500, XBTRT511, Terminals equipped with a matrix display and a touch screen with 10 lines x 33 characters.

(Answer based on Vijeo Designer Lite version 1.3)
Was this helpful?
What can we do to improve the information ?