Technical FAQs

Ask a Question

Can I configure the ATV312xxxx variable speed drives with PowerSuite?

Yes, ATV312xxxx drives can be configured with PowerSuite version 2.6, update patch 1.
Power suite has been updated over time so there are now patches 1 to 5 available , patch 5 was the last avaialble patch before the software was replaced by SoMove.
 
This update patch is available on the website: www.schneider-electric.com.
Fron the following location : http://www.schneider-electric.com/download/uk/en/results/0/0/8338608-PowerSuite-previous/0/?showAsIframe=false

Caution: This update patch does not take account of DeviceNet, CANopen daisy chain, or Profibus DP option cards.
Was this helpful?
What can we do to improve the information ?