Technical FAQs

Ask a Question

What is the part number of the label on TeSys U (LUB12 or LUB32)?

The part number of the label (8 x 18 mm) to be clipped on is LAD90.

NB: These labels are only sold in multiples of 100. 
Was this helpful?
What can we do to improve the information ?