Technical FAQs

Ask a Question

Which switch-disconnectors comply with UL standards?

There is a range of switch-disconnectors in the GS1 range that complies with standards UL98 and CSA22.2 no. 4.

This range is different from the standard range.
The part numbers for this range are given in the attached file.
Was this helpful?
What can we do to improve the information ?