Technical FAQs

Ask a Question

What adaptation parts satisfy standard UL 508 type E on the GV2P and GV3P?

The adaptation parts to be used so that GV2P and GV3P circuit breakers comply with standard UL 508 type E are detailed below.


For GV2P circuit breakers:

  • Order a GV2PxxH7(*) (except 32 A) circuit-breaker
  • Add a "Large Spacing" adaptor, part number GV2H7 Without this adaptor, the protection will not be certified UL 508 Type E
     

For GV3P circuit-breakers:

  • Order a GV3Pxx circuit-breaker
  • Add a "Large Spacing" cover, part number GV3G66 (to be placed on the power supply unit)
  • Add a signaling contact, part number GVAM11

 

For GV3P with connection by lug-clamps:

  • Order a GV3Pxx6 circuit-breaker
  • Add two IP20 covers, part number LAD96570
  • Add a signaling contact, part number GVAM11


(*) The only difference between GV2PxxH7 and GV2Pxx circuit-breakers is their marking

Was this helpful?
What can we do to improve the information ?