Technical FAQs

Ask a Question

What is the minimum bending radius of the connector cables and extension cables for sensors?

XZC** connector cables and extension cables for the following Schneider Electric detectors should be installed such that minimum bending radius quoted below is observed;
 

  • XU** photo-electric
  • XS** inductive
  • XX** ultrasonic







  • With flexing of the cable: Minimum bending radius = 15 x external diameter
  • With static operation of the cable: Minimum bending radius = 10 x external diameter
  • For bare cables type XZCB4L****: Minimum bending radius = 3 x external diameter
Was this helpful?
What can we do to improve the information ?