Technical FAQs

Ask a Question

Which combination block is used for circuit-breaker and contactor on the LAD311 mounting plates?

Between the following two products both mounted on the LAD311 plate: 
  • GV2ME/GV2P circuit-breakers,
  • TeSys D range contactors: LC1D09-LC1D38,
the combination block to be used to link the power connectors of the two devices is part number GV2AF4.
When the above two products are not mounted on the LAD311 plate, the circuit-breaker/motor combination block is part number GV2AF3.
If it is an LC1K range contactor, the combination block to be used between this range of contactors and the above circuit-breakers is GV2AF01.
Was this helpful?
What can we do to improve the information ?