Technical FAQs

Ask a Question

Does the Icm of Masterpact NW, apply to both symmetric and asymetric faults?

Icm is the maximum value of the asymmetrical short-circuit current that the circuit-breaker can make (symmetric value will be a lower value, so it will be covered as well)
Please check page 10 of attached pdf (or printed page 8 of the same file).
Was this helpful?
What can we do to improve the information ?