Technical FAQs

Ask a Question

Which PLCs are programmed using the PL7-2 software?

PL7-2 software is used to program:

  • The TSX17-20 with a language cartridge
  • The TSX27
  • The TSXP47-10, TSXP47-13, TSXP47-20 modules
PL7-2 software is used for programming in Ladder and Grafcet languages.
Was this helpful?
What can we do to improve the information ?