Technical FAQs

Ask a Question

What position should the address selector have to connect directly to a TSX NANO PLC with PL7-07 on the Terminal port?

To connect directly to a TSX NANO PLC with PL7-07, check that the dial on the terminal socket is set to address 0.
Was this helpful?
What can we do to improve the information ?