Technical FAQs

Ask a Question

What is the part number of the transfer cable between a PC and a TSX17?

The part number of the transfer cable between a PC and a TSX17 is TSX17ACCPC.  This cable includes an RS232/RS485 converter and has a 9-way SUBD connector on the PC end and a 15-way SUBD connector on the TSX17 end.

This product is no longer on general sale and is only available from our Services and Projects division.
Was this helpful?
What can we do to improve the information ?