Technical FAQs

Ask a Question

What is the possible substitution for XUVH003530 - XUVN0243R?

This is an obsolete system comprising an amplifier and interchangeable optical heads for a variety of applications. Such a system no longer exists in the Schneider range although in most cases there is available an application specific product that, whilst not a like for like replacement, can be used to perform the same function.

XUVH003530: Amplifier for optical heads, 3-wire PNP, light or dark programmable switching, 12-24 VDC power supply.
XUVN0243R: Thru-beam fork sensor, sensing distance 0.02 m between jaws, green transmitter/receiver
 
Substitution
This combination photoelectric thru-beam fork sensor and amplifier unit is replaced by a single product with built-in amplifier:

XUYFNEP60030 or XUYFANEP60030 optical fork sensor with learning function: both products have two 3-wire outputs and two PNP and NPN outputs. Adjustable sensitivity.

As these are not "like for like" replacements, it is necessary for the customer to ensure these devices are suited to the application. More data can be found on the attached document

Was this helpful?
What can we do to improve the information ?