Technical FAQs

Ask a Question

What is the content and what are the advantages of the various "Include" projects installed by default with Vijeo Citect?

The "Include" projects installed by default with Vijeo Citect contain predefined elements which can be used in application projects.
"Include" projects are:

  • The Include project, contain predefined elements included with Vijeo Citect versions prior to version 5.0 (templates, genies, super genies and symbol libraries).
  • The CSV_Include project contains predefined elements utilised in the XP style template pack.
  • The CSV_InstantTrend project is a preconfigured project allowing the use of instant trends.
  • The Tab_Style_Include project contains the new template packs available in v7.20.
Was this helpful?
What can we do to improve the information ?