Technical FAQs

Ask a Question

Why are the Digital Inputs for PM8000 meters not counting correctly?

Relays are normally susceptible to bounce, which means when the switch closes the arm can bounce on the contact  causing the load's power to flicker slightly. hence the pulse counter may incorrectly interpret a bouncing relay contact as a multiple switch event. Could you please check the Debounce setting as per the attached snapshot below:
Was this helpful?
What can we do to improve the information ?