Technical FAQs

Ask a Question

Can EGX300 be used with a PM5341 meter?

Direct ModbusTCP devices have to be defined in Remote Device Connections in order to view logged data from PM5341, these steps should be followed:

- Manually add the PM5341's IP address in the Remote Device Connections list;
- Manually add PM5100/PM5300 device type on the previously entered IP, now selectable from the drop-down combo;
- Add a unique Local ID in the range 1..247
- Add the address 255 in the last field, Remote ID; allowable values are 1..247 and 255.

When you enter 255 and press "Apply" button, the field will become empty, but the values will show up correctly if you'll try to trend them.
Was this helpful?
What can we do to improve the information ?