Technical FAQs

Ask a Question

Can You Export Logged data from an ION7650 using ION Set up software?

Yes, ION Setup is a option for a simple application to download the Ion 7650 internal logs.
If you connect to the meter using the Data Screens, you will be able to monitor real time quantities, and on the Data Recorders folder you will find the Data Recorder Viewer pager, just open one of the pages and all the data logged by the meter on that data recorder will be downloaded.
Once the download is completed you can copy all the content and paste on another document, for example an excel spreadsheet. It is not an export function, it should be done by copying and pasting the data into another file.
Was this helpful?
What can we do to improve the information ?