Technical FAQs

Ask a Question

Can the Zs value of NSX 100F be adjusted?

The Zs value for any NSX breaker of 160A rating or less with a TMD trip have a fixed magnetic trip, the long time (Ir) setting of 70% to 100% effect tripping times up to 10000 second. which is out side the time required for 0.4 and 5 second disconnection.
Was this helpful?
What can we do to improve the information ?