Technical FAQs

Ask a Question

What are the Dimensions of the MG6CEXM meter kit?

The meter extension box for the syle C powerpact 4 boards ( MG6CEXM) = HWD 200 x 850 x 260mm. This is the same width and depth as the board but will add 200mm in height.
Was this helpful?
What can we do to improve the information ?