Technical FAQs

Ask a Question

Do we offer 20Amp NSX breakers?

We only offer 20Amp NSX breakers in 1 & 2 pole devices, for 3 & 4 pole devices you will need a 25A device and adjust the thermal down to 0.8 (i.e 25 x 0.8 = 20A). The breaker will then be set at 20A.
Was this helpful?
What can we do to improve the information ?